alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon
Swagelok Kansas City | Little Rock | Omaha | Quad Cities

Authorized Swagelok Sales and Service Center

Differential Instrumentation Impulse Lines: Ensure Accurate Readings Through Proper Installation

Tap Location

Ensure Accurate Readings Though Proper Installation

Tap LocationSwagelok products are commonly used to hook up differential pressure transmitters to measure flow, level and pressure. Here are some simple guidelines to ensure your installation will provide accurate measurements. Assuming a horizontal process line, the first step in ensuring an accurate measurement is proper placement of the pressure connections. We will consider three different types of measurements: Gas, Fluid and Steam.

First, let’s consider a gas application. Imagine a line bisecting your process pipe vertically – that is running from 12:00 to 6:00. Ideal tap location is 45˚ on either side of this line at 12:00, with one tap on each side (Figure 1).

Tap LocationNext we will look at fluid measurements. Again we will bisect our process pipe but this time horizontally. Ideal tap location is 45˚ below the horizontal line, on either side of the pipe (Figure 2).

And finally steam measurements. Once more we are going to put the tapping points in the upper half of the pipe, 45˚ on either side of the 12:00 position (Figure 3).

Next let’s consider where we are going to mount the instrument. For our gas measurement we want to mount the instrument above the process pipe. This way any condensation which might occur will drain back into the process pipe, rather than accumulate in the impulse line. A good rule of thumb is to slope the lines 1:10 to help the condensation to drain and to avoid sharp bends or creating “traps” where condensation could build up. Provide tube supports if there is vibration. As a good practice, support ¼” through ½” tubing every three feet.

Tap LocationFor liquid measurements, we want to mount our instrument below the process pipe. Again, a 1:10 slope is ideal. Special care must be taken to ensure we don’t have sharp bends or traps where gas bubbles can build up. Once more provide tube supports if there is vibration. As a good practice, support ¼" through ½” tubing every three feet.

For steam measurements, while our tapping points are above the process pipe, we are going to mount our instrument below the process pipe. We want to mount two condensate pots or wells above the process pipe. Ideally these will be mounted at the exact same height, so that the impulse lines running from the condensate pots to the differential pressure transmitter have the same exact difference in elevation- this simplifies our calibration procedure. Impulse lines will run from the low point on the condensate pot to the high and low connections on our differential pressure transmitter. Once more a 1:10 slope is good to encourage trapped bubbles travel up to the condensate pots. The condensate pots are filled with water to the same level, as are the impulse lines running to the differential pressure transmitter.

Following these simple rules will help ensure the accuracy and repeatability of your transmitter readings.

View more Articles

This document was prepared by Swagelok Kansas City | Little Rock | Omaha | Quad Cities. The information and recommendations are intended as general information only, are subject to change without notice, have not been verified by Swagelok Company, and do not contain or create any warranty or guarantee regarding accuracy or completeness. Users bear responsibility for determining the suitability of information, recommendations, and products for their own use and situations. Consult catalogs on www.swagelok.com for the most current information about Swagelok products and services.