alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon
Swagelok Kansas City | Little Rock | Omaha | Quad Cities

Authorized Swagelok Sales and Service Center

Gas Chromatograph Installation: Understanding the Sample System Design Basis

Gas Chromatograph Installation

Understanding the Sample System Design Basis

Say for instance an EPC is contracted for a refinery upgrade for a new hydrotreater, which includes the installation of a brand new gas chromatograph (GC) in the upstream crude unit, designed for simulated distillation set up to measure end point temperature. Part of this new project calls for the sampling of four separate liquid streams, with sample tap locations that require exceedingly long sample lines (200-500 feet) to the projected analyzer shelter location.

Gas ChromatographThe GC will select in revolving sequence a sample from each of these liquid streams and inject to the GC for analysis. As we should all know by now, the analyzer itself is likely a reliable and well constructed device for its intended function. The analyzer, however, cannot be placed in the middle of the process line for in-situ analysis. Interestingly, more advanced in-situ spectroscopic methods of analysis continue to gradually permeate the market. In the future, such installations may eliminate much of the headache associated with the process sampling and conditioning system. For the time being, however, the selected GC will reside in a remote sheltered location and needs to be on the receiving end of a properly conditioned sample. No small task.

Complicating matters is a design basis calling for a one-minute fast loop transport from sample tap to shelter. On the surface, this would appear to be a sensible request; you certainly do not want to be taking yesterday’s sample. Timeliness of a sample system response is always of paramount consideration.

As we often see, however, the process engineering component to analyzer sampling is critical, and warrants a view into the wider picture of plant operations. Considering the intended purpose of the analyzer, how critical is the one-minute transport time?

Where did one minute come from? Will these results directly inform a control algorithm making process changes by the minute, or factor into wider blending considerations done manually on more of a daily basis? What if we challenge the design basis and find a more prudent approach that ultimately meets the project objectives without over-engineering a sample system?

Scoping out various options for techno-commercial analysis – the same practice fully required for the new hydrotreater unit, for instance – is well warranted for new analyzer configurations. Moreover, these analyzer studies warrant the attention of both a process engineer and analyzer/I&C engineer.

ChromatographIt’s likely that we could reduce capital and operating costs if we recognize that a one-minute transport time – on a stream that will be analyzed only once every 30 minutes – is simply not that critical. We can make use of standard fast-loop modules and reduce the amount of fastloop flow. We can utilize smaller transport lines and put in smaller conditioning components. We can buy a smaller shelter. How often are system integrators able to identify this issue and then have the wherewithal to take “exception” and propose an alternative? How cognizant are plant or EPC process engineers of design basis criteria or requirements? How involved are they when establishing project scope for these sample systems? 

 

The parent process unit is heavily simulated and engineered from a process engineering standpoint. There are well-defined specs on product requirements that are to be achieved across a range of potential feedstocks. The sampling process is a miniature version of this, designed to achieve a certain temperature and pressure (almost always different than at the sample location) at the analyzer within a desired and useful amount of time. Unlike the parent process unit, the sampling system is often not nearly as thoroughly engineered, resulting in ill-conceived and imprudent analyzer installations, consuming operations man-hours and at times even wasting capital.

Understanding how the big picture relates to an analyzer’s ultimate purpose can be key to its successful installation. Using that knowledge to inform an appropriate design basis for the sample system is one of the most important first steps to ensuring that purpose is met.

View more Articles

This document was prepared by Swagelok Kansas City | Little Rock | Omaha | Quad Cities. The information and recommendations are intended as general information only, are subject to change without notice, have not been verified by Swagelok Company, and do not contain or create any warranty or guarantee regarding accuracy or completeness. Users bear responsibility for determining the suitability of information, recommendations, and products for their own use and situations. Consult catalogs on www.swagelok.com for the most current information about Swagelok products and services.