alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon
Swagelok Kansas City | Little Rock | Omaha | Quad Cities

Authorized Swagelok Sales and Service Center

Process Analyzers: Improving Overall Reliability

Process Analyzer

Improving Overall Reliability

Grab Sampling SystemModern-day analyzers are sophisticated and refined instruments, but they still have a stigma of poor reliability. While the quality of the analyzers has most definitely improved, there still exists some doubt about the overall reliability of sampling systems. Lore within the sampling community says you could expect 80% of the overall analyzer downtime to be the result of issues within the sample system (Clevett 1986*). Luckily, this leaves an obvious way to improve overall analyzer reliability! In the next few sections, we will discuss some main reasons sample systems can cause issues in analyzers, why we should care about this, and what we can do to improve the systems.

Sample systems are the facilities to extract, condition, and transport a sample from process to the online analyzer. Each of these steps has the potential to wreck the reliability of the analyzer. The designer must consider how the sample interacts with each component along the entire journey from tap to analyzer and how this may impact the reliability of the system as a whole. Sample systems are not very tolerant of design error; each error compounds, and eventually, the analyzer is plugged or exposed to incompatible process conditions. To design a reliable sample system, the designer must consider the entire path from process tap to the analyzer and how each component affects the sample as it travels through the system.

Even if the system were designed correctly, process conditions could change. A small change in pressure, temperature, or makeup could send the entire system spiraling into unplanned downtime costing the plant every minute. Whether facilitated through a third-party or in-house a simple way to monitor the process sampling conditions is to perform regular audits of the sampling system and sub-components and keep a record of their condition.

Often overlooked, the sample system is vital to utilizing the analyzer to its full engineered capacity. The sample system is the first line of defense in protecting the analyzer and providing it a representative and reliable sample. While a sample system might be orders of magnitude cheaper than the analyzer, an investment in correctly designing the sample system will only pay dividends down the line in overall reliability and analyzer performance.

* Clevett, Kenneth J. Process Analyzer Technology.
John Wiley & Sons, 1986.

View more Articles

This document was prepared by Swagelok Kansas City | Little Rock | Omaha | Quad Cities. The information and recommendations are intended as general information only, are subject to change without notice, have not been verified by Swagelok Company, and do not contain or create any warranty or guarantee regarding accuracy or completeness. Users bear responsibility for determining the suitability of information, recommendations, and products for their own use and situations. Consult catalogs on www.swagelok.com for the most current information about Swagelok products and services.